2020-07-01 8:24 AM
I want to get an STM3210E-EVAL Board. It is mentioned in the eval board overview that the used stlink is ST-Link V3/E. But in the ressources i cant find any reference to it.
Do i need to buy an ST-Link V3/E to debug the Hardware, or is the ST-Link onboard like the nucleo versions?
Also the new ST-Link V3 is modular. Would i need specific modules?
Fast Help appreciated
2020-07-01 8:32 AM
STM3210E-EVAL does not have a built-in STlink. JTAG/SWD is available as 2 20 Pin connector . Stlinkv3 and Stlinkv2 have the corresponding connector, as does a JLINK and many other debuggers.
2020-07-02 11:49 PM
But why does it mention STLink V3E here :
For me it is just a question of do i need an extra Debugger or not. A JTAG 20 Pin port is there so i can easily use it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.