2025-11-21 9:36 AM - last edited on 2025-11-21 9:44 AM by Andrew Neil
Hello Everyone,
I would like to get recommendations for STM32 development kits that have at least 3 DACs with their 3 independent outputs exposed, preferably a newer kit that can run an RTOS (not Linux). The faster the better.
Thank you!
Solved! Go to Solution.
2025-11-28 5:02 AM
I assume I cannot "Accept as Solution" but one of the answers above. But, both @TDK and @MasterT had answers I wanted and was looking for and am most grateful for. I have purchased both boards and will try the newer/faster one first (NUCLEO-H7A3ZI-Q) and see if it will do what I need. If not, I'll fall back to the other one (nucleo-G474re).
@Andrew Neil : If I just counted on AI, I'd still want verification from an experienced person. Still, the AI has been helpful for injecting new ideas. Thanks!
Thanks!
2025-11-21 9:49 AM
You might try asking the new "Sidekick" AI assistant ...
STM32 Sidekick: the AI-powered tool that accelerates your design journey
2025-11-21 9:51 AM - edited 2025-11-21 9:56 AM
NUCLEO-H7A3ZI-Q has independent DAC outputs on PA4-PA6 which are all exposed. Two outputs are on DAC1 but they are independent.
I don't think any STM32 chips have 3+ DACs that all support external output, but if you just want independent outputs, the above will work, among others.
2025-11-21 3:25 PM
nucleo-G474re has 2 regular buffered dacs, than +4 fast 15 msps buffered by internal opa's. Total 6.
Not sure it can run RTOS
2025-11-22 7:31 AM
Hi @TDK ,
I noticed you replied to this other forum question regarding the NUCLEO-H7A3ZI-Q.
Do you know if it is now possible to use all 3 DAC channels simultaneously?
Thanks!
2025-11-22 8:07 AM
I don't have that board to test, but I see no reason why it can't work. Peripherals are independent. A DAC output not working at all is not an issue that would get pushed to production silicon.
2025-11-28 5:02 AM
I assume I cannot "Accept as Solution" but one of the answers above. But, both @TDK and @MasterT had answers I wanted and was looking for and am most grateful for. I have purchased both boards and will try the newer/faster one first (NUCLEO-H7A3ZI-Q) and see if it will do what I need. If not, I'll fall back to the other one (nucleo-G474re).
@Andrew Neil : If I just counted on AI, I'd still want verification from an experienced person. Still, the AI has been helpful for injecting new ideas. Thanks!
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.