2016-05-03 7:35 AM
Is it possible to feed only the MCU on top of a Nucleo board without powering also the embedded ST-Link? I tried, but unfortunately the only solution seems to manually remove the connection between the ST-Link and the MCU reset line (plus removing the power line to the ST-Link). I would propose a more simple configuration, maybe adding an easily operable jumper like the EXT5V or USB5V selector. If anyone knows a simplier way, please let me know
#st-link #nucleo #hardware #swd2016-05-03 9:41 AM
Which Nucleo? The Nucleo-144 boards are very easy to power externally. Got one here wired to a 7VDC 1.8A supply so I can run a Cellular Modem off it. Jumpered it to use VIN
Not clear what ''on top'' means, the ST-LINK part is at the top of the board with the silk-screen/parts naturally orientated. There have been issues with older ST-LINK firmware holding devices in reset, but this have been addressed in current versions. To run a Nucleo-64, you might need to modify it a bit, but I doubt this is more than removing a handful of parts.2016-05-04 2:52 AM
Hi Fabio_IT,
Yes, it is mentioned in Nucleo user manual: If the board is powered by USB (U5v) both jumpers JP1 and JP5 are as follow: JP1 is ON JP5 is on pin 1 pin 2 If you want to power the Nucleo using external power supply connected to E5V or Vin jumpers should be : JP1 OFF JP5 on pin 2 pin 3 Note that to connect Vbat pin to VDD, the solder bridge SB45 hsould be ON. Refer to the Nucleo user manual for more hardware details. -Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.