2025-11-06 7:32 PM - last edited on 2025-11-14 8:04 AM by mƎALLEm
Post edited by ST moderator to be inline with the community rules for the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code.
Hi,
I’m now trying to port the STEVAL-STWINBX1 firmware to my custom hardware whose MCU is STM32U575VGT6.
I started by porting the data logging application:
fp-sns-datalog2\STM32CubeFunctionPack_DATALOG2_V3.1.0\Projects\STM32U585AI-STWIN.box\Applications\DATALOG2
During execution the following code gets stuck,and eventually returns HAL_ERROR.
/* Wait for calibration completion */
while (LL_ADC_IsCalibrationOnGoing(hadc->Instance) != 0UL)
{
wait_loop_index++;
if (wait_loop_index >= ADC_CALIBRATION_TIMEOUT)
{
/* Update ADC state machine to error */
ADC_STATE_CLR_SET(hadc->State, HAL_ADC_STATE_BUSY_INTERNAL, HAL_ADC_STATE_ERROR_INTERNAL);
__HAL_UNLOCK(hadc);
return HAL_ERROR;
}
I’ve verified that the hardware is fine with my own test program (DAC generates a sine wave, ADC samples it, and I print the data over USART). I’m not sure what’s wrong—could you give me some suggestions?
zefang
2025-11-14 7:24 AM
Hello @dzf
I've just downloaded your example and started debugging. I'll come back to you in a few days.
Best regards,
Simone
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.