2023-10-30 12:16 AM
Hi there,
I have developed my project long time with MB1364E, exactly with H723ZG.
Now I have got my own PCB with H743. I would like to use ST-Link V3 (SWD) from Nucleo board just the same as it works for cuttable ST-Link from L4 Nucleos, e.g.:
https://community.st.com/t5/stm32-mcus-boards-and-hardware/how-to-use-the-standalone-st-link-capability-of-my-nucleo-after/td-p/306461
I have removed JP4 "Idd measurement", JP2 "Power source selection" and JP5 "Power selection".
But it seems that Nucleo ST-Link is hardcoded to support only this board.
Log from CubeProgrammer:
07:59:18:504 : UR connection mode is defined with the HWrst reset mode
07:59:20:007 : ST-LINK SN : 003600453331510B33323639
07:59:20:007 : ST-LINK FW : V3J12M3
07:59:20:008 : Board : NUCLEO-H723ZG
07:59:20:008 : Voltage : 3.29V
07:59:20:008 : Error: ST-LINK error (DEV_TARGET_HELD_UNDER_RESET)
07:59:20:024 : Disconnected
However, when my PCB is not supplied I get another error from CubeProgrammer, the voltage is correctly 0.00V detected:
08:03:06:200 : UR connection mode is defined with the HWrst reset mode
08:03:06:234 : ST-LINK SN : 003600453331510B33323639
08:03:06:234 : ST-LINK FW : V3J12M3
08:03:06:235 : Board : NUCLEO-H723ZG
08:03:06:235 : Voltage : 0.00V
08:03:06:235 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
08:03:06:249 : Disconnected
Yes, I can still work with external ST-Link V3 and my board. But I also want to reuse part of not anymore used NUCLEO board.
Let's say, just to reduce garbage and save the world.
Is there a way to free the ST-Link V3 from NUCLEO board?
Solved! Go to Solution.
2023-10-30 5:51 AM - edited 2023-10-30 5:52 AM
looking at the circuit (MB1364) , the H723 is fix connected to the st-link F723.
so no easy way to use it.
you could try cutting the connections swdio, swclk, swo (sb32) close to the H723 and use the CN5 pinheader to connect a cable.
but maybe it expect just a H723 as target...and refuses to work with other.
2023-10-30 5:51 AM - edited 2023-10-30 5:52 AM
looking at the circuit (MB1364) , the H723 is fix connected to the st-link F723.
so no easy way to use it.
you could try cutting the connections swdio, swclk, swo (sb32) close to the H723 and use the CN5 pinheader to connect a cable.
but maybe it expect just a H723 as target...and refuses to work with other.
2023-11-29 2:20 AM
Hello @DrDro
Check the user manual STM32H7 Nucleo-144 boards (MB1364) - User manual
It should be helpful as well.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-29 7:15 AM
>> but maybe it expect just a H723 as target...and refuses to work with other.
I'm not aware about such a limitation, so far...
Anyways, for that board, the use case is that you can only bring an external probe to debug the H723, but can't debug an external MCU with the on-board ST-Link V3.
Maybe it is possible, but as you said, there is some work to do with cutter/soldering iron.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.