2019-07-25 8:58 PM
Nucleo-G474RE has JP7, which pulls down BOOT0 pin to ground when a jumper is installed, but this alone does not control boot options. What is the intended usage of JP7? Does it have something to do that Nucleo-G474RE comes with nSWBOOT0 option bit cleared?
2019-07-26 2:11 AM
Well, the jumper allows to pull PB8-BOOT0 low. It give you options to play with.
2019-07-26 6:52 AM
Dear Yoichi,
Yes you are right, on this board, by default, the option bytes are set with nSWBOOT0=0 and nBOOT0=1.
Meaning that, in this case, pin BOOT0-PB8 is not used for BOOT configuration, and you can use PB8 as normal I/O.
You are free to set back nSWBOOT to 1 thanks to STM32CubeProgrammer and use PB8 for BOOT configuration.
2019-07-26 6:58 AM
PB8-BOOT0 is active high when used as BOOT0; pulling it down doesn't have any effect in this case. For using PB8-BOOT0 as GPIO, why this particular pin is provisioned for pull down?
2019-07-26 7:00 AM
Yes. I understand the nSWBOOT option. My question is about "an intended usage of JP7".
2019-07-26 7:01 AM
Yes. I understand the nSWBOOT option. My question is about "an intended usage of JP7".
2019-07-26 7:11 AM
When nSWBOOT=1, and JP7 is fitted, it allows to pull-down BOOT0/PB8, and avoid having BOOT0 floating.
When nSWBOOT=0 and JP7 not fitted, you can use PB8 on CN5 or CN7.
2019-07-26 8:00 AM
Okay, so JP7 should be fitted to keep BOOT0 from floating in nSWBOOT = 1 mode.
This suggest G4's BOOT0 behavior is different from predecessors like F4, in which BOOT0 could be left floating at any time?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.