2024-03-24 10:55 AM
I am trying to write code to enable the MCO1 clock output on pin PA8 on the STM32H755ZIT6U microcontroller, the code is fairly simple.
The code below is my attempt to do so. I couldn't find the problem.
/**
This code activates MCO1 and MCO2 so we can probe the clock frequecy of the STM32 MCU
**/
#include "stm32h755xx.h"
int main(void){
// enable the clock to AHB4
RCC->AHB4ENR &= ~(RCC_AHB4ENR_GPIOAEN | RCC_AHB4ENR_GPIOCEN); // reset
RCC->AHB4ENR |= (RCC_AHB4ENR_GPIOAEN | RCC_AHB4ENR_GPIOCEN); // enable clock
// set PA8 as alternate function
GPIOA->MODER &= ~(GPIO_MODER_MODE8_0 | GPIO_MODER_MODE8_1); // reset
GPIOA->MODER |= (GPIO_MODER_MODE8_1); // AF
// set PC9 to alternate function
GPIOC->MODER &= ~(GPIO_MODER_MODE9_0 | GPIO_MODER_MODE9_1); // reset
GPIOC->MODER |= (GPIO_MODER_MODE9_1);
// set the speed of PA8 and PC9 to very high speed
GPIOA->OSPEEDR |= (GPIO_OSPEEDR_OSPEED8_0 | GPIO_OSPEEDR_OSPEED8_1);
GPIOC->OSPEEDR |= (GPIO_OSPEEDR_OSPEED9_0 | GPIO_OSPEEDR_OSPEED9_1);
// set the alternate function of PA8 and PC9 to AF0
GPIOA->AFR[1] &= ~(GPIO_AFRH_AFSEL8_0 | GPIO_AFRH_AFSEL8_1 | GPIO_AFRH_AFSEL8_2 | GPIO_AFRH_AFSEL8_3);
GPIOC->AFR[1] &= ~(GPIO_AFRH_AFSEL9_0 | GPIO_AFRH_AFSEL9_1 | GPIO_AFRH_AFSEL9_2 | GPIO_AFRH_AFSEL9_3);
// set the MCO1 to HSI
RCC->CFGR &= ~(RCC_CFGR_MCO1_0 | RCC_CFGR_MCO1_1 | RCC_CFGR_MCO1_2);
// divide the output by 15
RCC->CFGR |= (RCC_CFGR_MCO1PRE_0 | RCC_CFGR_MCO1PRE_1 | RCC_CFGR_MCO1PRE_2 | RCC_CFGR_MCO1PRE_3);
while(1);
}
I tested it by configuring the clock tree in CubeMX and it worked, the output is about 4.2MHz, which is what I expected, but I couldn't do the same without the autogenerated code.
2024-03-24 11:26 AM
Ahlayn @FadiEid and welcome to the ST Community :smiling_face_with_smiling_eyes:.
What i suggest you is to debug step by step the code generated from CubeMX. Then follow which registers are configured in each step. After that, reproduce it using the register programming.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-24 11:54 AM
Hey man, I will do this. I just thought there is something obviously wrong in my code and decided to reach out for help. shoukran
2024-03-24 12:02 PM
Sure there is something wrong on your code. What i suggest you is the best way to do it.
If you are looking for any other details. You can always create new posts on our community for each request habibe.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.