2023-11-06 2:09 AM - edited 2023-11-06 2:09 AM
Hello everyone, I'm trying to set all the pins(except 11) of port F of STM32L476 as Analog to save power.
for(uint8_t GPIO_PIN = 0; GPIO_PIN < 16; GPIO_PIN++)
{
if(GPIO_PIN != 11) GPIOF->MODER |= (3 << (GPIO_PIN * 2));
}
But it resets my program while executing these lines.
Solved! Go to Solution.
2023-11-06 2:37 PM
(1) What are the port F pins connected to externally? Or what internal peripherals are they (normally) connected to? Have you disabled the internal peripherals before this? Use your debugger, step through the loop and see which pin causes the reset.
(2) Why the loop? Why not just write 0xff3fffff to GPIOF->MODER?
2023-11-06 2:37 PM
(1) What are the port F pins connected to externally? Or what internal peripherals are they (normally) connected to? Have you disabled the internal peripherals before this? Use your debugger, step through the loop and see which pin causes the reset.
(2) Why the loop? Why not just write 0xff3fffff to GPIOF->MODER?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.