2026-04-23 12:11 AM - last edited on 2026-04-23 2:44 AM by Andrew Neil
hello ST Community,
There's an STM32 board in a USB pen drive format with a small flash memory capacity and only a few pins (3-5 pins) for UART serial communication. On this STM32 board, inside the USB pen drive, I can program the dedicated software for serial communication.
If it exists, can you tell me the model and serial number? I can't find it online.
Thanks for the information.
Solved! Go to Solution.
2026-04-23 1:22 AM
You probably mean a so-called Blue Pill of an Asian manufacturer, which has, for many years now, only been produced with counterfeit MCUs. Desperate users who wanted to save a few cents regularly ask in the Community for a solution to the major problems they have with it.
There are two ways to avoid these problems:
A NUCLEO always comes with a debugger as well, so the apparent price advantage quickly vanishes.
And they are guaranteed to work flawlessly.
Hope that helps?
Regards
/Peter
2026-04-23 1:22 AM
You probably mean a so-called Blue Pill of an Asian manufacturer, which has, for many years now, only been produced with counterfeit MCUs. Desperate users who wanted to save a few cents regularly ask in the Community for a solution to the major problems they have with it.
There are two ways to avoid these problems:
A NUCLEO always comes with a debugger as well, so the apparent price advantage quickly vanishes.
And they are guaranteed to work flawlessly.
Hope that helps?
Regards
/Peter
2026-04-23 2:37 AM - edited 2026-04-23 2:38 AM
2026-04-23 2:45 AM
@Domy_ST wrote:There's an STM32 board in a USB pen drive format with a small flash memory capacity and only a few pins (3-5 pins) for UART serial communication.
Is that supposed to be a question ?
2026-04-23 4:38 AM
yes, what's wrong?
2026-04-23 4:39 AM
Thanks
2026-04-23 4:57 AM
You wrote it as a statement: "There is..."
So you meant a question: "Is there... ?"
2026-04-23 5:01 AM
Yes, you're right, I didn't notice. It was a typo.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.