2019-05-07 12:44 AM
I'm using ST-LINK_CLI to flash my STM32F427 and I'd like to start SWO tracing after flashing. Is there a (Windows) command line tool which can do this? Currently running Win7, ST-LINK CLI v3.4.0.0 and ST Link FW: V2J33S7
2019-05-07 6:35 AM
Hello,
J-Link commander should be able to do this but you'd need of course to use a J-Link probe. Note however that you can turn most onboard ST-Links into J-Link (and revert them back) as described here: st-link-on-board
As an alternative, you could use openocd and this tool: https://github.com/robertlong13/SWO-Parser
There's also a pretty interesting and full-featured open source tool for SWO tracing named Orbuculum but unfortunately it runs on Linux and OSX only.
2019-05-07 7:45 AM
Hi.
STLink utility supports trace view with fixed freq 2MHz.
PB3 pin must be connected to SWO pin of STinkV2.(plus all the others for SWD)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.