2020-12-15 3:42 AM
Hello guys,
I'm very new to STM32s so please bear with me. Any help would be greatly appreciated. I am currently making a scratch-built STM32 board. I soldered on an STM32F407VET6 onto a QFP100 breakout board and I'm wiring together a minimal system on a through-hole protoboard. I used this schematic of a cheap STM32 board I bought as a reference design and also constantly referred to ST's official design guidelines. I believe I made a proper "minimal setup" required for my STM32 to run properly. However, when I plug it into my computer, nothing is detected. I know I have the proper USB drivers installed because my STM32 discovery board works fine. Here is what I've done so far:
Here's what I didn't do so far:
After many hours of head-scratching and frustration, I'm gassed out. I can't possibly think of anything else I might've missed. Maybe my chip is defective/fried, but I didn't do anything to it that could've fried it. So please, help a brother out! Again, I am pretty new to STM32s, so thank you for staying with me and any help is welcome!
Thanks!
P.S. I figured photos wouldn't be much help at all since my wiring job is absolutely atrocious and it wouldn't give any useful info. But if y'all want it, I can certainly post it here. Oh also, in case you're curious, I'm making this custom board to prototype my design for a custom PCB using the same chip.
2020-12-16 2:42 PM
> I just want to see if my laptop detects the STM32's USB DFU mode when it's plugged in.
So, does it?
2020-12-16 2:51 PM
Make sure VDDA is powered.
If you don't have a scope or meter, using a flying lead to an LED. Perhaps have one wired high the other low.
Check if NRST is clamped low or now.
If the clock doesn't start the USB won't be used. People tend to wire up the debug headers so they can check functionality/responsiveness there.
With a USART1 on PA9/PA10 you could check for signs of life sending a 0x7F pattern at 9600 8E1
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.