2017-09-17 7:11 AM
Hi All,
I am trying to use STM 32 ST-LINK utility to flash my .hex code to STM32L4 microcontroller on my custom board using SWD. I have tried all the modes under Target Settings (Normal, Hot Plug, Connect Under Reset) without any luck. With hot plug selected, I think, I can connect to the microcontroller, it displays ID, flash size etc. but I can not erase chip or write hex code because it displays 'Read out protection is activate'. If I try to open Option Bytes, it gives me error but ends up displaying the window anyway. On the window, read out protection is set to level 1. In this mode I can make changes on the GUI but can not save them, because of the protection, so I am stuck in a never ending loop, I think. Can you please let me know what needs to be done so that I can fix this issue and able to write hex code to my microcontroller using ST-LINK/V2?
Thanks!
Dushyant.
#st-link/v22017-09-18 1:49 AM
I don't know the 'official' way to do this.
The way I do this is to download some code to RAM which disables readout protection.
I don't know how you'd specify building a project to download directly into and execute from RAM from your development environment.
But my code essentially does:
Old version:
int main(void) { FLASH_Status protector; FLASH_OB_Unlock(); FLASH_OB_WRPConfig(OB_WRP_Sector_All, DISABLE);/* protector = */FLASH_OB_RDPConfig(OB_RDP_Level_0); protector = FLASH_OB_Launch(); FLASH_OB_Lock(); logU(protector); logString(' Unlock Complete\n'); return 0;}Newer version:uint32_t SystemCoreClock;int main(void) { SystemCoreClock = 16000000; HAL_InitTick(TICK_INT_PRIORITY); /* Unlock the Flash to enable the flash control register access *************/ HAL_FLASH_Unlock(); /* Unlock the Options Bytes *************************************************/ HAL_FLASH_OB_Unlock(); HAL_StatusTypeDef rc = FLASH_If_WriteProtectionConfig(OB_WRPSTATE_DISABLE); if (rc == HAL_OK) { /* Generate System Reset to load the new option byte values ***************/ HAL_FLASH_OB_Launch(); /* Lock the Options Bytes *************************************************/ HAL_FLASH_OB_Lock(); debug_printf('Successful'); } logString(' Unlock Complete\n'); return 0;}Hope this helps,
Danish
2017-09-18 8:33 AM
Thanks Danish for the reply,
no, I don't have a code which can load code to RAM instead of Flash, but I will try yours to fix the issue I am having.
Is this normal though? to have SWD pins disabled for a microcontroller? I don't know how eval board gets around this problem.
Thanks,
Dushyant.
2017-09-19 10:13 AM
I did not have correct connections made in my custom board, that was the problem.
Thanks Danish.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.