2020-10-19 12:22 PM
Hello, Got a stm32H750B discovery board and it kills me as i don't fully understand.
I managed to understand a bit with the help of clive, as right now when i try to connect with STLINk v2 on the SWD connection i get a STM32F72X chip recognised (not the board itself).
Is it possible to flash this chip in order to make it the board functional again?
Thanks,
Bogdan
2020-10-19 2:38 PM
Had you erased the F723?
Does the PC currently recognize the ST-LINK/V3 when plugged into CN14?
2020-10-19 11:59 PM
The F723 seems to be empty.
PC does not recognise the STLINK. when i plug the usb inside the STLK connector, there is no activity - the LD4 should be lighted, but it is dead.
2020-10-20 9:10 AM
Did you perhaps not remove JP3 and the F723 is still under reset?
2020-10-20 9:38 AM
No, JP3 is unset.
Tried to reset F723 by setting JP3. It is under reset, but still no difference :(.
It is very likely i removed the firmware on F723. Don't know how i managed to do that. Tried several times to force H7 to reset bootloader, however it does not work.
2020-10-20 10:04 AM
I am quite sure the STLinkV3 bootloader is RDP1 protected. From V37 on, the SWD access to the F723 is closed. Try to access the F723 via CN5 with another adapter.
However I guess you somehow applied voltage above VCC of some F723 pin and that killed the F723...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.