2024-12-29 8:54 AM
Hi,
I'm trying to get started with the STM32 NUCLEO-H7S3L8 board to create a USB HS device. I am new to the boot/application split development (also to trustzone) and don't know where to find the right resources to get started. I have tried using the STM32CubeIDE examples importer but keep receiving "failed to copy error" which I don't know how to debug. I have also tried loading the project from the git repo, I can compile and run the boot project but know how to properly setup the application project to run as well.
I would really appreciate some pointers on where to find the information to get the CDC_Standalone example running and how to develop with the boot and application.
Apologies I can't be more specific, I seem a little out of my depth and don't know where to start!
Solved! Go to Solution.
2025-01-14 11:21 AM
After reading around for a considerable time I discovered that the STMCube code generator always sets the USB reference clock to 24MHz (unfortunately I have mis-placed the link to the post) which then conflicts with the HAL USB Init.
The problem was fixed by setting the USBPHYC Clock Mux to use the NUCELO-H7S3L8 external 24MHz HSE.
2024-12-30 2:18 AM
Hello @Linduri, welcome to ST Community,
Here are some solid resources you can start from to understand the boot/application split development;
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-30 10:37 AM
In addition to the links above, here you can help and support with your STM32 project.
2025-01-14 11:21 AM
After reading around for a considerable time I discovered that the STMCube code generator always sets the USB reference clock to 24MHz (unfortunately I have mis-placed the link to the post) which then conflicts with the HAL USB Init.
The problem was fixed by setting the USBPHYC Clock Mux to use the NUCELO-H7S3L8 external 24MHz HSE.
2025-02-16 6:19 AM
Hello @Linduri,
Could you please share your minimal working USB Device ioc file if possible ?
I am trying to setting it up without success...
Thanks,
s.
2025-02-17 9:15 AM
2025-02-17 12:54 PM - edited 2025-02-17 12:58 PM
Thanks, @Linduri.
My setup is quiet different, taken from the CDC_Standalone.ioc example, so booting from external flash and USB HS Device. I also think that UCPD setup is required for this purpose (CDC_Standalone.ioc enables it by default).
I will also test yours.
s.
2025-06-01 1:13 PM
Thanks for sharing it, it was usefull, now my laptop is able to see CN2-USB
Watching many videos but the boards were diferent and the configuration don't match, more in Clock Configuration
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.