2021-07-04 5:18 PM
Hi, I've come across a few of these issues namely here but I haven't found a fix for my issue yet. I have a custom PCB based on the STM32H745ZIT6 chip which I wired up to be powered using the LDO power supply. However, I'm running into two problems at the moment:
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}The Configuration function is shown here:
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Macro to configure the PLL clock source
*/
__HAL_RCC_PLL_PLLSOURCE_CONFIG(RCC_PLLSOURCE_HSE);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 1;
RCC_OscInitStruct.PLL.PLLN = 60;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 5;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
{
Error_Handler();
}
}Regardless of me using the external HSE or the HSI, it doesn't make any difference at all. the program just hangs at the lne where it's waiting for the power flag.
My other issue is Cube IDE doesn't even bother to generate the peripheral clocks within ClockConfig but I guess this is moot if I can't configure the main core anyway.
Has anyone managed to find a fix for this?
2021-07-05 6:11 PM
The best suggestion from here was to run a CubeMX example that runs at 480MHz and see what it does and if it works.
https://community.st.com/s/question/0D50X0000BVpWdp/stm32h747-freezes-waiting-for-vosrdy
Report back if you figure it out please. I'm sure it's something dumb or undocumented.
2021-07-05 6:47 PM
I managed to figure it out. I generated the same project for a h745-nucleo board which I'd modified for LDO and that worked fine. Turns out I just needed to change the power supply for my PCB. For some reason, the clocks won't initialise with this powerbank I use even though it works with my other STM32 devices.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.