2022-02-01 7:44 AM
Hello, I have been trying for a while to test the STMCube programming chain up to the STM32F411 via the STLink without success despite all the ideas read in the forum. During a review of the requirements for the installation of CUBE it is noted, under Windows, WIN 7, 10 but not 8 or 8.1. Too bad, 8.1 is my OS. I attach the error message that it returns to me systematically. Thanks for your help !
Error in final launch sequence: Failed to start GDB server
Error in initializing ST-LINK device.
Reason: (17) Could not find an ST-LINK with serial number 310061000E00004637364D4E.
Please verify the serial number in the debug c
PS: the serial number is the same as the one present when opening STM32 LINK utility
2022-02-01 8:52 AM
Hello
It is an STM32F411 Discovery board ?
Can you connect to the F411 with the ST-Link Utility ?
2022-02-04 10:51 AM
Hello, no I am using STM32f411 black pill. And yes I can connect without problem with STM Link utility. Have a nice day and thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.