2018-06-28 3:48 AM
Hello there,
Does anyone uses the external loader of the ST-Link tool for the STM32L073xx micro-controller (MC)?
What we would like to do:
We have a board based on the
STM32L073rz. On this board, we have an EEPROM connected through I2C to the Micro-controller. We would like to use the external loader of the ST-Link tool to read and write the EEPROM.
The problem:
When we use a command of the external loader (e.g. read) , we get this error: 'The elf loader is bigger than the RAM size.' .
We think that this error message means that ST-Link is trying to load into the 20k RAM and does not have enough space. It seems that the HAL and GPIO software takes most of the space, but we were not able to shrink either HAL or GPIO. We would like to know if anyone was successful doing this , and how to achieve it.
Regards
#stm32l073 #st-link #external-loader2018-06-28 4:53 AM
I've written several loaders, if the abstraction you are using is too thick, then you'll need to use a thinner one.
The loader and a data buffer need to fit within the RAM constraints.
Make sure the HAL isn't pulling in the floating point libraries. I recall the USART driver pulling it in, others might too.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.