2025-01-22 3:35 AM - last edited on 2025-01-22 3:36 AM by Andrew Neil
Im using Nucleo-H755 i have using this board for the last 3 months usually i get some Errors like no target found but i have solved those by viewing in the community chats but this Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication i have tried every thing i know and suggestions in the other posts like connect under reset , boot0 high , power down mode but i couldnt get it connected while connect the board there is a file in the H755 storagenamed FAIL.txt in that this msg is present The interface firmware FAILED to reset/halt the target MCU is there any other way to flash the board
Solved! Go to Solution.
2025-01-26 11:47 PM
@Vimal_M_A wrote:
yes im sure i always set smps only
Sorry I didn't understand. The issue I mentioned previously is indeed when you set the power in SMPS but CubeMX set both SMPS and LDO. Check your project preprocessor.
2025-01-22 3:40 AM
What tool & version are you using to do the flashing - STM32CubeProgrammer?
Are you using the onboard ST-Link?
What does it show for the Target voltage?
2025-01-22 4:28 AM
17:56:58 : ST-LINK SN : 001A003F3233511739363634
17:56:58 : ST-LINK FW : V3J15M7
17:56:58 : Board : NUCLEO-H755ZI-Q
17:56:58 : Voltage : 3.26V
17:56:58 : Error: Unable to get core ID
17:56:58 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
2025-01-22 4:29 AM
Thanks.
What tool & version are you using to do the flashing - STM32CubeProgrammer?
2025-01-22 4:33 AM
Try STM32CubeProgrammer with Reset Mode Under Reset. This might help in cases where a bad firmware disconnectes the SWD debug interface or goes to some low-power modes soon *after* reset.
You may also play with the other settings, like reducing the speed.
hth
KnarfB
2025-01-22 4:43 AM
tried that also still not able to connect
2025-01-23 8:21 PM
Is there any other way to flash the Microcontroller
please let me know
2025-01-24 1:32 AM
Use the System Bootloader?
2025-01-24 5:50 AM
can you explain how to do that
2025-01-24 6:10 AM - edited 2025-01-24 6:13 AM
Hello,
Are you sure you set SMPS instead of LDO for power configuration on this board (Nucleo-H755)?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.