2022-12-25 11:59 PM
Hi team,
I need to use transceiver(AD9361, 70M-6GHz) to complete some design. I found that most solutions are based on FPGA as processor.
I want to ask whether STM32 could be as a baseband processor and communicate with AD9361 or not. If it is workable, could you recommend related device?
Thanks!
2022-12-26 2:05 AM
Check the data rate of the ad chip, and the interface. Check if the bandwidth is compatible. Core frequency will need to be at least higher to process the data, because at minima data should flow... check STM32H7 series.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.