2025-02-15 9:25 AM
All of a sudden, I cannot connect to this board via stlink usb cable. I tried pressing reset button, updated firmware, connect in every possible mode (hardware reset, core reset). Is there a combination/sequence of pressing buttons? In other stm32 mcu I saw a way to erase memory by connecting a resistor to reset pin and ground momentarily. Can this be done on this board and how? Anything else i can try before I trash it? Thank you for your help!
Solved! Go to Solution.
2025-04-06 7:16 PM - edited 2025-04-06 7:16 PM
OMG! I must have accidentally slid off the little plastic jumper connector connecting JP4 off of the pins. (Not an electrical guru here.) I only noticed it when comparing to an identical board that I subsequently purchased thinking I must have damaged this one. Anyhow, the plastic connectors that slide onto both JP4 or JP3 are important -- I was not able to established connection to the board without either one.
2025-02-25 6:41 AM
Hello @psabela,
Could you try with another USB cable? Which error did you get?
I recommend you to look at these FAQs:
These articles describe tips to prevent or fix errors encountered when connecting the STM32 target board to your computer.
I hope this will help you to solve the issue.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-06 7:16 PM - edited 2025-04-06 7:16 PM
OMG! I must have accidentally slid off the little plastic jumper connector connecting JP4 off of the pins. (Not an electrical guru here.) I only noticed it when comparing to an identical board that I subsequently purchased thinking I must have damaged this one. Anyhow, the plastic connectors that slide onto both JP4 or JP3 are important -- I was not able to established connection to the board without either one.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.