Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Subject edited to mention ARM64 - p.a. Hi everyone, I am having trouble getting my STM32 NUCLEO - F411RE setup. When I attempt to run a simple program through CubeIDE I am met with "NO ST-LINK detected! Please connect ST-LINK and restart the debug se...
Hi! I'm using a STM32N657 Nucleo Board, and, considering the 1.8 V reference voltage for the ADC, the value returned by the ADC is half of what it should be. For example, for a 1,410 V value in the pin, the reading is 1742. Here is the initialization...
Hello, I purchased an STLINK-V3PWR from Mouser. When I tried to use it, STM32CubeIDE 2.1.1 suggested updating the firmware. This failed, and the STLINK-V3PWR appears to be unusable (bricked). What can I do? Return the device for a refund/replacement?...
Hi everyone, I’m designing my first custom PCB for an underwater ROV project (Leak Detection + ESC Control + Jetson Interface) and I would really appreciate feedback before moving closer to manufacturing. A few months ago I shared the schematic revi...
I recently bought a STM32F446 64 pin chip and wired it up. The following circuit is made: I've installed 0.1uF capacitors between two power pins, and two I've not (It's difficult to do so) it's consuming around 20 to 30 mA Pin 30 shows 1.132 volts ...
Hello, I am designing a USB-C power sink using the TCPP01-M12 and STM32G071CBT6 (UCPD peripheral). The connector is a Molex 2171790001 receptacle. I have two separate issues and would appreciate guidance on both. --- ISSUE 1: No power at all with Typ...
Hi! I am working on a design that uses an SD card and an STM32U5 MCU. In trying to educate myself more thoroughly about SDIO bus design, I've come across LVS (low voltage signaling), which is part of the UHS-I spec and required for reaching SD speeds...
I have a Nucleo-WL33CC1 board which has been working fine, but after starting to work on a DEEP SLEEP implementation I can not connect any longer using SWD neither through Crossworks IDE nor CubeProgrammer. Any possibility to unbrick the board?
I have used a Micro USB cable and it doesn't insert. Help
Hi, I wanted to set up time keeping on my Discovery board for testing something. I see the following in the documentation for the larger STM32F769-EVAL: https://github.com/STMicroelectronics/STM32CubeF7/blob/master/Projects/STM32F769I_EVAL/Exampl...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.