Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi, im planing on running computer vision DL models on multiple STM32 boards. At this moment I will compare a STM32MP256F-EV1 with a STM32H747-DISCO, however i only bought the B-CAMS-OMV and is not the same connector on the MP board. IS there any way...
Hi, We have bought the NUCLEO-H533RE board and I tried to power it via E5V by connecting the Arduino Minima R4 board 5V power output into E5V and GND signals in pins 6 an 8 respectively. I instantly noticed that the LED LD3 is lit with green, but the...
I am having difficulty creating AD schematic and PCB libraries for the NUCLEO-H563ZI from the MB1404 Altium project files. The process fails when attempting to create similar components, such as resistors.Is there any chance of obtaining the librarie...
Hi everyone ! I am having problem with the I²C connection. The problem is that, normally the the SDA and SCL pins work properly (I checked it with a logic analyzer) but when I connect them to the module or sensor I use, both of them goes LOW and stay...
I’m testing low-power modes on my STM32 B-L072Z-LRWAN1 board and measuring the current consumption. When I measure the current using a Xiao PowerBread, I get around 20 mA on the 5 V rail, even when the MCU enters Sleep Mode. My question is whether th...
Hi everyone,create the cubeide project for onboard PDM MEMS microphone on stm32 discovery kit. 1- I2S22-Mode: Half Duplex Slave3-DMA Settings -> add -> SPI2_TX Problem in section 3 . I cannot see the SPI2_RX which I will get the PDM peripheral to mem...
Hello I tried a blinky code which works with an other disco board I bought several months ago and it doesn't work with the new one. I tried it in debug mode and I'm stuck here.void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /...
Dear Team,I would like to know if development kit is available for STM32H7B0VBT6 if yes where can I purchase the same ? Also I would like to know does the stm32 workspace support this microcontroller (STM32H7B0VBT6) if yes can you help me with the d...
Hello Everyone, I have the Nucleo-H7S3L8 as my first STM32 board. I want to connect it to a Segger J-Link Pro for JTAG. In the official documentation (https://www.st.com/resource/en/user_manual/um3276-stm32h7rx7sx-nucleo144-board-mb1737-stmicroelectr...
Purchased the SensorTileBoxPro and got in way over my head. I wanted a wearable to detect and alert of undesirable head movement. 1. Can this device be programed to do this?2. Is there anyone that could program it for a modest fee?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.