STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Hi, I can't connect to STM32F030R8T6 using ST-LINK V2 and STM32CubeIDE on Ubuntu 18.04.5 LTS.

I use STM32F030R8T6 and an interface card that plugs into a breadboard for direct prototyping, ST-Link v2 STM32 and STM8 Programmer, both from Newbiehack.com.Connected as on photo: SWDIO to pin 46 (PA13), SWCLK to pin 49 (PA14), GND to pin 62, 3.3V t...

Adam_K by Associate II
  • 14249 Views
  • 6 replies
  • 0 kudos

Is there a way to power a nucleo 64 board from a 3V external battery without damaging the board?

Hello,I'd like to power my nucleo L152RE from a 3V external battery.I thought this should be easy but then I read that some soldering needed to be done? Is that true? I'd like to be able to power the board from an external 3V battery to use it as an ...

BCora.1 by Associate III
  • 4536 Views
  • 7 replies
  • 0 kudos

How to program flash directly thru SWD?

Hi, Everyone,I am developing the standalone SWD programmer operating by battery.I have a problem to program flash thru SWD directly.So, I traced SWD line with the ST-Link Utility. It looks that some tiny flash program code and updated user firmware a...

paul0208 by Associate III
  • 9100 Views
  • 9 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.