Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I need 16 DAC outputs for my project. I was planning on using Texas Instrument's DAC8168IAPW over I2C and making a daughter board to connect to the Disco board. I also plan on adding an IC to drive LEDs. Do I power the daughterboard using the Disc...
I used the STM32CubeIDE for 3 years on a Windows10 PC. After installing the 8-bit ST_Tools (STM8CubeIDE,...) on the same PC the connection to a NUCLEO-64 (STM32-G431RB) does no longer work. Now STM32CubeProgrammer reports "No ST-Link detected". Howev...
Please link to the schematic. Is there any input with a pull-up resistor up to 5V?Please link to the schematic. Is there any input with a pull-up resistor up to 5V?
Hi,I am using ST-LINK_CLI for flashing mcu via ST-Link ->SWD. In ST-Link utility can be set Reset mode (SW,HW,Core). How can I set this parameter in ST-Link_CLI ? I did not find anything in documentation.Or is there any better tool to control STLin...
Hi,I'm completely new to MCU programming, so I designed a simple board with a STM32f103c8t6 to program with the Arduino IDE. I flashed a bootloader from the STM32duino Github.But when I plug my board to my computer, the status led flashes, but the bo...
I see numerous examples of 4-wire SWD without a reset pin connection.I come from the PIC world where there is always Data, Clock and Reset for a Pgm/Dbg interface.I bought a Chinese STLink-V2 programmer/debugger and it has a reset pin as well as data...
Hi,today I got my STLINKV3-MINIE and I quite like the polarized 14-pin Flat ribbon connector that is used on it.I searched a bit, but could not find this exact type of connector this is: Does anybody know what make and model this is?Thanks!Oh, and wh...
Is it a problem to set the constant of the external pull-up resistor connected to the "PB9_Boot0" signal to 100kΩ? (R13)Also, if there is a problem with the connection, I would like you to point out the relevant part.
I would like to use the STM32F779AI, in WLCSP package. I did not find any application notes, or schematics or dev board for such MCU. Is there some litterature or example, schematics, ... talking about layout rules, VIAs, etc... for the WLCSP-180 (p...
On the board schematics the LED is just connected to PJ2.I configured pin PJ2 as GPIO output push-pull, state high. So it should be off. But after roughly 1 second from reset the LED turns on and blinks like every 20 seconds.It's supposed to be user ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.