STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Boot0 Tied to SWCLK on STM32G0B1KET6 MCU

Hello, I am making the connections for programming the STM32G0B1KET6 in hardware and came across the boot0 pin sharing the same connection as the SWCLK for serial wire debug (I am using the 32 pin version of this mcu). Just to confirm to program the ...

0693W00000WIxFxQAL.png
DSopp.1 by Associate
  • 2996 Views
  • 1 replies
  • 0 kudos

PROBLEM Debug project with external loader

Debug project with external loader Hi all,I have a project with an external loader and I didn't succeed to enter to debug and download the hex (sometimes is and sometimes it is not it didn't consistencyi didn't understand if it's the st programmer or...

NBita.1 by Associate II
  • 3198 Views
  • 5 replies
  • 0 kudos

Resolved! STM32L433CCT6 Datasheet DS11449 Rev 6 (page 21) - Concerning power up/power down phases in hardware design

Hi, can someone refer to the above MCU reference. This is my first time using the STM32 MCU chip on my embedded system. My question regarding the power up/down phases concerning specifically on STM32L433CCT6 IC ... Is it a must and critical to use so...

STehA.1 by Associate II
  • 2919 Views
  • 4 replies
  • 0 kudos

Why brand new Discovery boards give me "Error: failed to erase memory" when I am just loading up the ST provided demo hex

I have 4 Discovery boards:STM32F769I-DISCO, STM32F469I-DISCO, STML4R9I-DISCO, and a STM32H747I-DISCO boards. The H7 and L4 boards came pre-loaded with the demo firmware. So I downloaded the ST provided demo hex files for both the F4 and F7 boards. Us...

TStra.6 by Associate II
  • 1469 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.