Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
While trying to disable TZEN on a NUCLEO-WBA52CG boar after running the GPIO_IOToggle_TrustZone Example an both LEDs working as expected i encountered the error Error: ST-LINK error (DEV_TARGET_NOT_HALTED)after switching from RP Level 1 to RP Level 0...
/* USER CODE END Header *//* Includes ------------------------------------------------------------------*/#include "main.h"/* Private includes ----------------------------------------------------------*//* USER CODE BEGIN Includes */#include <string....
The board is newly purchased from ROBOKITS INDIA, and i received it about 4 days back, now when im connecting it to my laptop, it gives an error saying device descriptor failed, now i tried to do the other solutions like uninstalling the driver, rest...
STMicroelectronics ST-LINK GDB server. Version 7.5.0Copyright (c) 2023, STMicroelectronics. All rights reserved.Starting server with the following options:Persistent Mode : DisabledLogging Level : 1Listen Port Number : 61234Status Refresh Delay : 15s...
I am using the Stm32H747I-DISCO board for the x-cube-ai application, working with the FP-AI-VISION1 package. I already updated the package that suits the board version and read the user manual UM2611, according to the instructions I ran the code and ...
I need to know STM32H7 Wafer Size please
I have a timer that generates an event out on:1. DAC to generate sine wave.2. ADC to read the sine wave and do FFT.Question 1:I find that the fundamental frequency of the sine wave is as follows:Counter value = ((Timer peripheral clock/desired freque...
I am debugging a firmware for force measurement in STM32f429i in STM32 Cube IDE and TouchGFX. In that I am using ili9488 LCD driver with tsc2004 touch sensor. My issue is on the display screen I couldn't navigate to next pages i.e., touch is not dete...
I have a new "Nx_MQTT_Client" sample application that I had set up and working on the B-U585 board. I tried it on another board I had, and it said I needed to update the WiFi BIOS. It had previously been updated to v2.11.1.I got the latest download, ...
i am working in a project on stm32u5a9j-dk board. i am fetching temperature value from inbuilt temperature sensor using ADC channel. I am getting the value in 4 digit int. i want to know to know how to transfer that value into *celcius. And one more ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.