Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
i am trying to connect "RFID YHY502CTG" with STM32F407G-DISC1,i have attached the datasheet of RFID,please help me to send and receive data. i am using this code in while loop.while (1){/* USER CODE END WHILE */ /* USER CODE BEGIN 3 */Txdata[0]=0xAA;...
Hi everybody,I am trying to use the audio on stm32f746g-disco.I can hardly find a tutorial for this.Many solutions got their way to solve it and left not much details.lots of the solutions guide to the examples in CubeMX , but they seems a little bit...
I want to pair the STM32 BL475E IoT01A to a HC05 module connected to another STM32F401ccu6 to send data to the IoT board.But when I tried to do so,I'm not able to find the pairing key anywhere.I tried 0000,1234,1111 but that didnt work.Is there any o...
Hi,at this url https://www.st.com/en/evaluation-tools/nucleo-wl55jc.html#tools-softwarethe download of the demo binary result in a zip that is corrupt.ThanksM.
I am currently utilizing the Nucleo U575 board for a proof-of-concept endeavor. My aim is to power up the board via an external power supply input. Specifically, I've opted to use the 5V_USB_C from the USB Type-C® connector (CN15) for this purpose.I'...
In the context of a research project, I am using the STM32H743ZI2 microcontroller for object detection. However, I lack prior experience with camera interfacing and configuration. I am using a B-CAMS-OMV camera module. Therefore, I would be grateful ...
I have a H563ZIT6 . I attach its I3C(used as target) to an I3C controller, and then i find that there is no register for static address in target mode in I3C of H563ZIT6, i just find DEVR0 for dynamic address. Does I3C of H563ZIT6 support static addr...
Hi everyone,I am running en.x-cube-spin14 sample code for X-NUCLEO-IHM14A1 (STSPIN820 stepper motor driver) on a nucleo64 board with STM32F411REBefore any move of the stepper motor this code is executed: if (HAL_GPIO_ReadPin(BSP_MOTOR_CONTROL_BOARD_...
Hi,tried to update the ST-Link Firmware on my NUCLEO-F429ZI as requested by STM32CubeIDE. Updating failed and the board is no longer recognized as a USB device. The COM LED (LD4) on the ST-Link section blinks red.Is there a way to resurrect the firmw...
Hi everyone.I am developing an application on STM32H723ZGT6, I am trying to connect LwIP with ADC at DMA and also an SPI.So these three things are my main componenets that I am running on FreeRTOS.1: At SPI I want to transmit multiple commands at 60k...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.