Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
STM32H750 Discovery Kit board, Timer 1, Ch1 (PA8 output) I used direct access to timer registers as a HAL library and the result was similar. I can receive 10 MHz with direct access to register and TIM1->PSC = 10; But when I set TIM1->PSC = 1 I do...
hello NXP Expert, I am trying to achieve the maximum speed for the ST7735S 1.8 inch TFT, but it's very slow on the STM32 microcontroller. However, it reaches maximum speed with the NXP controller. In the video below, you can...
Hello, I need a to find a Nucleo board with 2 12-bit ADCs and at least 2.4 MHz sampling frequency. I also need an integrated external phy for HS usb2.0 data transfer. Which STM32 boards are in correspondence with these requirements? Thanks in advance...
We have a part on our custom board which includes a STM32L072CZ. The part was shipped with obsolete firmware, and we are trying to upgrade the firmware with the new image provided by the manufacturer. We first tried to upgrade the firmware using Se...
I have attached the code below could some one help me please
Hi,We are currently working on a design involving the STM32U5G7VJT6Q microcontroller and would appreciate your expertise in reviewing the power section of our design. I have attached a diagram of the power section for your reference.Could you please ...
I once made a prototype pcb that contained a Nucleo-32 G431. During testing, I noticed that the PCB did not work and even contained a short circuit. On closer inspection I noticed that the rows of the Arduino Nano connectors on my PCB were swapped. F...
wondering what these pins do as the shutter goes to the 1v5 regulator input and the flash comes from the strobe pin and while I'm at it what motor is af-vcc for thanks for the help
Hello ST Community - I am looking for example projects in order to evaluate the various sensors and peripherals, including the display. I did check here: https://github.com/STMicroelectronics/STM32CubeH5/tree/main/Projects/STM32H573I-DKAre there any ...
Hello Currently i'm using STM32F769I-EVAL board with on-board debug unit ST-LINK/V2-1. I would like to know whether ST-LINK/V2-1 firmware is open source & freely available for end user ?Could someone hint ? Thanks. RegardsBivin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.