STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Could someone suggest me a board?

Greetings.I have a project I developed on ESP32 (CH340 Chip). For some reasons, the project got messy, and I would like to migrate to a new board. I have an STM32 Nucleo which gave me a lot of satisfaction, but for this project I need something-Small...

MMast.11 by Associate III
  • 2893 Views
  • 5 replies
  • 6 kudos

Resolved! Battery powered B-U585I-IOT02A

I'm building a simple application that collects environmental data from sensors (pressure, temperature and humidity) using the B-U585I-IOT02A development board. Since I want to deploy the node directly on the field, I'm planning to power the board us...

Resolved! ADC not filling all the buffer with DMA

Hi, I'm using a Nucleo-H723 board and I need to sample 4 ADC's with variable sampling rate, maximum 1Mbps.I configure the TMR2 with the time stamp (10ms, 1ms, 10ms, etc...), and TMR3 with the sampling rate that is the input for the ADC trigger.Values...

fposser by Associate III
  • 6795 Views
  • 6 replies
  • 2 kudos

STM32H7S78-DK: Examples needed

Hi all,Anyone have example projects for the following for the STM32H7S78-DK board ?:1)"Hello World". Displaying the text "Hello World" on the display.2)Audio. Playing back a simple tone though the audio output.Am new to development so the included di...

mfny by Associate III
  • 3935 Views
  • 6 replies
  • 2 kudos

STEVAL-IDB008V2 add service error

Hi all, I'm trying to test STEVAL-IDB008V2 board with wise studio and BLE_SensorDemo project I can compile and flash with RF-Flasher.So for now I'd like to add my own service, the basic example privde 2 services - Acc service- Env serviceI'm trying t...

SBaro.11 by Associate III
  • 1365 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.