Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello I think we can control the reset and boot0 pin of F407 externally through a different board STM32H745 disco. I want to put the F407 in boot mode and send data to program the F405 through UART. Please confirm Thanks & Regards, Anuj
Hello, I have created a custom PCB based on STM32U545RET6Q and I am getting crazy to do it work. I have a random errors and I can't solve any of them becaouse each time the hardfaluts are different. I started to work with the EVAL board MB-1841 (STM3...
Hi, I have a buffer with 65000 values in 16 bits from the ADC read that I need to provide to my computer running a python code.Any suggestion how can I handle this in both sides?I'm trying to use this function but I'm getting weird data when I'm list...
I encountered an issue where an error occurs when only the image data is moved to NOR Flash in the linker. I have already verified that the NOR Flash works correctly in a separate project by toggling the LEDs.In my current TouchGFX project, I enabled...
Hi,Although I'm quite familiar with Arduino and Teensy MCU's, I'm just getting started with STM32. I followed this 'getting started' video to upload an Arduino bootloader to my STM32F103C5T6 'blue pill' module, using an ST_LINK module.Before uploadi...
Hi All,I've been using my ST-LinkV3mini for a few weeks now quite happily, until two days ago when it just stopped talking to my M3 MacBook Air (MacOS 15.0.1). I'm fairly sure I know what's happening, when I try to communicate between the laptop and ...
Hi,When I try to generate code from stm32cubemx v6.4.0. I'm getting an error message like "The Eclipsec execution launcher was unable to locate its companion share library.". I'm attaching the screen shot here How to resolve this issue Thanks,Akhil
(STM32F407)I use an ADC with 2 channels, I should use that way. I want to save the bits separately, like in the example below. How should I configure MINC?Is MINC working like this?After the first conversion is complete:The value of Channel 1 is writ...
Hello everyone,We recently ordered an STM32F407VET6 board for our project because the specific board we needed wasn’t available. However, we’re now concerned about the authenticity of the board and whether it might be fake. We’re encountering issues ...
We're using the STM32F407VET6 microcontroller. When I connect it to my Windows laptop and attempt to debug with STM32CubeIDE, it shows "NO ST-LINK DETECTED, CONNECT AND RESTART DEBUGGING." I’m unsure how to resolve this issue. The user manual states ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.