Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
HelloNow I use systick on STM32L0538-Discovery and I'd stop systick during RTC Power stop mode.Please show me hot to stop the systick and restart.Thanks
Split from: https://community.st.com/t5/stm32-mcus-boards-and-hardware/stm32h747i-disco-lcd-display-problem/td-p/643493 Hello, May ,I know how to enable the display. I am not getting how to on the backlight of the display
Hello STM32 Folks,I am currently working on a design that requires interfacing a high-density RAM (256 Mb or 512 Mb) with a microcontroller (STM32U5) via the HyperBus interface. The RAM module is powered by 1.8V, while the STM32U5 needs to be powered...
Dear SirThere is 24 Pin connector at development STM32L4P5G-DK. I am unable to find which LCD is compatible with with this 24 pin connector.Kindly suggest a part no of LCD
Hello!I've been working with several STM32 parts since 10 years. I'm working for a company so due to confidentiality I can't share the schematic of the custom PCB, sorry.On the first batches of a new product, using a STM32H743BI, it appears that some...
We are working on a project called 4G Testjig in which we have interfaced 4G module(EC25) with NUCLEO-F413ZH. We are powering the Nucleo board using micro-USB cable.We are testing GPIOs and UART of 4G module (EC25) on NUCLEO-F413ZH board using GPIOs ...
Hello! I am having trouble downloading a demo project to my STM3210E-EVAL evaluation board and am looking for help.I'm using IAR Embedded Workbench for Arm v9.60.3. From within this IDE, I downloaded the example project STM32F10E_EVAL_Demo. I'm using...
I have been using the generic stm32f407vgt6 discovery board as a programmer to program another stm32 board[stm32f103ret6]. I am able to do this by removing the 2 jumpers on the discovery board. While this works, stm32cubeide is unable to recognize th...
That's basically it. I'm thrown off because this page explicitly says it has a 'CAN FD Transceiver', however, nothing says CAN on the silkscreen and this graphic I found: Refers to the D14 and D15 pins as "CAN TD" and "CAN RD", which I assume is TX...
In qorvo software package for DWM3000, they have provided a stm32 project, but it has been initiated for STM32F429 Nucleo board. I have STM32F446 Nucleo board, so how can i port that project to use with my nucleo board. Thanks in Advance !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.