2024-03-14 5:56 AM
Hello everyone, I hope you're doing well.
I'm starting a new project where the main requirement is Wi-Fi connectivity and connection to AWS IoT. While researching what ST has to offer in this regard, I came across the document: https://community.st.com/t5/stm32-mcus/getting-started-with-stm32u5-iot-discovery-kit-and-aws/ta-p/49682. It discusses the B-U585I-IOT02A kit, which seems to be quite comprehensive. However, I noticed that the code available in the document https://github.com/FreeRTOS/iot-reference-stm32u5.git entirely uses FreeRTOS and does not include the .ioc file, which I am quite familiar with for configuring pins, timers, etc.
Does ST have any other examples or kits that include Wi-Fi and AWS IoT connectivity? If yes, could you please provide a reference link? If not, I would like to know if it's possible to port the pure FreeRTOS code to a version that uses both FreeRTOS and the ST configurator .ioc.
Thank you.
Solved! Go to Solution.
2024-03-14 10:58 AM
Hello @ffjunq
For the configuration of the AWS support on the B-U585I-IOT02A, i suggest you to refer to the X-CUBE-AWS. All exemples that does not use cube MX can be migrated to use CubeMX including project with RTOS.
If you want to use another board with examples containing a .ioc fil, i suggest you to use the X-CUBE-AWS-H5 with the STM32H573I-DK.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-14 10:58 AM
Hello @ffjunq
For the configuration of the AWS support on the B-U585I-IOT02A, i suggest you to refer to the X-CUBE-AWS. All exemples that does not use cube MX can be migrated to use CubeMX including project with RTOS.
If you want to use another board with examples containing a .ioc fil, i suggest you to use the X-CUBE-AWS-H5 with the STM32H573I-DK.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-14 11:43 AM
Thank you for the support!
Do you happen to have the STM32U585 board ported for CubeMX? I'm asking because I don't have much time to dedicate to development, so I'm not comfortable spending time on porting. In this case, I believe it would be best to migrate to the STM32H5 board, as I'm more familiar with CubeMX configurations.
2024-03-14 12:02 PM
Unfortunately, all examples for the STM32U585 does not use CubeMX but you can regenarte. You may think about using the STM32H5 examples.if your question is answered, close the topic by choosing a best answer.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.