2019-11-06 7:47 AM
Hello!
In X-CUBE-NFC6 manual https://www.st.com/content/ccc/resource/technical/document/user_manual/group1/16/85/63/86/35/64/42/47/DM00635198/files/DM00635198.pdf/jcr:content/translations/en.DM00635198.pdf
i can see:
"2.1 Overview
The X-CUBE-NFC6 software package expands the STM32Cube functionality.
The package key features are:
• Sample application to detect NFC tags of different types and mobile phones supporting P2P, card emulation mode and read/write"
But in package i can't find this example. I can find only "WriteURI" example.
Where i can get "Sample application to detect NFC tags"?
Solved! Go to Solution.
2019-11-07 12:22 AM
Hi,
the package should have all that in e.g.
STM32CubeExpansion_NFC6_V1.0.0\Projects\STM32L476RG-Nucleo\Applications\PollingTagDetect\Src\demo.c, ndef_demo.c
Project e.g. in STM32CubeExpansion_NFC6_V1.0.0\Projects\STM32L476RG-Nucleo\Applications\PollingTagDetect\MDK-ARM
Regards, Ulysses
2019-11-07 12:22 AM
Hi,
the package should have all that in e.g.
STM32CubeExpansion_NFC6_V1.0.0\Projects\STM32L476RG-Nucleo\Applications\PollingTagDetect\Src\demo.c, ndef_demo.c
Project e.g. in STM32CubeExpansion_NFC6_V1.0.0\Projects\STM32L476RG-Nucleo\Applications\PollingTagDetect\MDK-ARM
Regards, Ulysses
2019-11-07 2:01 PM
Hello!
Thank you for your answer, i will try it.
2019-12-15 6:34 AM
I'm successfully implement my own EMV-kernel (Visa+Mastercard) using this example as a starting point. All works fine, thank you.
Now i need to change PINs, used for SPI communication with ST25R3916 (to upload program to my custom board):
NSS - PB0
IRQ - PC5
To do this, i made changes in spi.h:
#define BUS_SPI1_NSS_GPIO_PIN GPIO_PIN_0
#define BUS_SPI1_IRQ_GPIO_PIN GPIO_PIN_5
#define BUS_SPI1_IRQ_GPIO_PORT GPIOC
#define BUS_SPI1_IRQ_GPIO_CLK_ENABLE() __HAL_RCC_GPIOC_CLK_ENABLE()
But example stops working after this changes. Sometimes i can read ChipID register (0x2A), but nothing else.
I've made experiments on X-NUCLEO-NFC06A1 board.
What else i need to change in code to correctly change pins, used for spi communication?
2019-12-17 2:32 AM
Hi,
please provide logic analyzer traces of the issue to be able to inspect.
Regards, Ulysses
2019-12-23 2:32 PM
Hello!
Problem was in code, that automatically been generated by Cube. Fixed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.