2026-04-26 11:37 AM
I am currently working with the X-NUCLEO-NFC10A1 board and interfacing it with an ESP32 DevKit V1. While attempting to establish communication between the two, I have tried all SPI modes as well as different reset logic configurations, but I am still unable to get them to communicate properly.
I have included my Arduino test code below for reference, which I am using to verify the communication:
Please check in attachment section there is code file
Solved! Go to Solution.
2026-04-28 2:28 PM
Hi,
make sure VDD and VDD_IO are both provided to the X-NUCLEO-NFC10A1. Make sure the various GND pins are properly connected.
Could you also send a picture of your setup?
Strange to see MISO always at 1. Could you check MISO/MOSI have not been swapped?
Rgds
BT
2026-04-27 3:55 AM
Hi Abhishek_1305,
Please observe:
Attach a logic analyzer to CS,MISO,MOSI,SCLK,RESET. See that SPI is driven in the right mode according to DS.
If you see the right waveforms and still doesn't work: Double check the supply and the connections. If still not working: Please share the logic analyzer traces + picture of the setup and any other helpful information.
BR, Ulysses
2026-04-27 11:55 PM
Hi,
in your readReg code
uint8_t readReg(uint8_t reg) {
uint8_t val;
SPI.beginTransaction(spiSettings);
selectChip();
SPI.transfer(0x40 | reg);
val = SPI.transfer(0x00);
deselectChip();
SPI.endTransaction();
return val;
}
SPI.transfer(0x40 | reg); is likely not correct. See Table 3 in the ST25R200 Data Sheet.
A C driver library is available for the ST25R200. It is portable on different MCU (STM32 or other MCUs). It prevents the need to reimplement the driver from scratch. See the X-CUBE-NFC10 package or the ST25 embedded NFC library.
Rgds
BT
2026-04-28 12:15 PM
I am currently working on interfacing the ESP32 with the X-NUCLEO-NFC10A1 board over SPI, and I would like to share my setup along with the steps I’ve already taken.
Here is my current connection configuration:
I have also attached logic analyzer captures along with my latest code for your reference.
Attached image bytes when I am sending 0x3F register with MSB Bit high and it becomes 0xBF and it gives response 0xFF.
Additionally, I have experimented with all SPI modes by configuring different combinations of CPOL and CPHA, but I am still facing issues with proper communication.
Currently I am using this SPI mode
Mode 1 (CPOL=0, CPHA=1): Clock idles low, data sampled on falling edge.
Could you please review my setup and provide guidance on what might be going wrong or any additional configurations I should check?
2026-04-28 2:28 PM
Hi,
make sure VDD and VDD_IO are both provided to the X-NUCLEO-NFC10A1. Make sure the various GND pins are properly connected.
Could you also send a picture of your setup?
Strange to see MISO always at 1. Could you check MISO/MOSI have not been swapped?
Rgds
BT
2026-04-29 11:45 PM - edited 2026-04-30 8:14 AM
Hi,
things to check:
Ulysses
2026-05-02 12:38 AM
Dear STM Community Support Team,
Thank you for resolving my issue so quickly. I appreciate your support and assistance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.