cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-C071RB Example with X-NUCLEO-NFC12A1 not working

Bassem
Associate II

Dear ST colleagues,

I tried recently the package X-CUBE-NFC12.

First I tested on NUCLEO-L476RG board the delivered example and it was working out of the box, then I tried on NUCLEO-C071RB but it was not working, first I noticed that the Pins configuration are not correct it was fixed, but still not working, did anyone ever test this example, because I assume it needs to work without any modification.

Thank you in advance for your support.

Best regards

Bassem Taamallah

1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

Hi,

I guess this is due to the polarity of the user button on NUCLEO-C071RB vs. NUCLEO-L476RG (active high vs. active low)

See https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/integrate-nfc08a1-expansion-board-with-stm32-u575zi-q/td-p/745862  

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Brian TIDAL
ST Employee

Hi,

I guess this is due to the polarity of the user button on NUCLEO-C071RB vs. NUCLEO-L476RG (active high vs. active low)

See https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/integrate-nfc08a1-expansion-board-with-stm32-u575zi-q/td-p/745862  

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.