2023-03-14 4:59 AM
int main(void)
{
/* USER CODE BEGIN 1 */
uint8_t nfc_data[32] = {0};
const uint16_t nfc_addr = 0x10; // NFC存储区的起始地�?�
const uint16_t nfc_size = sizeof(nfc_data); // NFC存储区的大�?
char* write_data = "Hello, world!"; // 待写入的字符串
char read_data[32] = {0}; // 读�?�到的字符串
// 将待写入的字符串�?制到nfc_data数组中
strncpy((char*)nfc_data, write_data, sizeof(nfc_data));
// 将nfc_data数组中的字符串写入NFC存储区
NFC07A1_NFCTAG_WriteData(NFC_INSTANCE, nfc_data, nfc_addr, nfc_size);
// 从NFC存储区读�?�数�?�到read_data数组中
NFC07A1_NFCTAG_ReadData(NFC_INSTANCE, (uint8_t*)read_data, nfc_addr, nfc_size);
// 打�?�读�?�到的字符串
printf("Read data: %s\n", read_data);
return 0;
/* USER CODE END 1 */
/* �?�片机�?置--------------------------------------------------------*/
/* �?置所有外设,�?始化闪存接�?�和 Systick。*/
HAL_Init();
/* 用户代�?开始�?始化 */
/* 用户代�?结�?��?始化 */
/* �?置系统时钟 */
SystemClock_Config();
/* 用户代�?开始 SysInit */
/* 用户代�?结�?� SysInit */
/* �?始化所有已�?置的外设 */
MX_GPIO_Init();
MX_NFC7_Init();
/* 用户代�?开始 2 */
/* 用户代�?结�?� 2 */
/* 无�?循环 */
/* 用户代�?开始于 */
而 (1)
{
/* 用户代�?结�?�于 */
MX_NFC7_Process();
/* 用户代�?开始 3 */
}
/* 用户代�?结�?� 3 */
}
/**
* @brief系统时钟�?置
* @retval 无
*/
Solved! Go to Solution.
2023-03-21 11:21 AM
Hi,
see https://community.st.com/s/question/0D53W00002BCNySSAX/code-to-read-and-write-ndef-on-xnucleonfc07a1 for similar question
Rgds
BT
2023-03-21 11:21 AM
Hi,
see https://community.st.com/s/question/0D53W00002BCNySSAX/code-to-read-and-write-ndef-on-xnucleonfc07a1 for similar question
Rgds
BT
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.