2020-03-09 6:31 AM
Solved! Go to Solution.
2020-03-09 9:42 AM
Dear customer,
Indeed ST25TV02K-AD has several features that are of interest for protecting the wine industry about counterfeiting. For example,
* An unique digital signature is stored on the tag to authenticate the product (see TruST25™ digital signature)
* The data stored in the tag can be either read-only, or protected by password for read and/or write.
* it offers the capability to detect that a wire connected to the tamper pins is open or closed, helping in protecting physically the content of the wine bottle.
* the tag can be permanently killed so that an opened bottle can never be used again as a valid product.
Have a good day.
Regards
2020-03-09 9:42 AM
Dear customer,
Indeed ST25TV02K-AD has several features that are of interest for protecting the wine industry about counterfeiting. For example,
* An unique digital signature is stored on the tag to authenticate the product (see TruST25™ digital signature)
* The data stored in the tag can be either read-only, or protected by password for read and/or write.
* it offers the capability to detect that a wire connected to the tamper pins is open or closed, helping in protecting physically the content of the wine bottle.
* the tag can be permanently killed so that an opened bottle can never be used again as a valid product.
Have a good day.
Regards
2020-03-09 10:30 AM
Dear JP,
Thank you very much for your time and answer. How could i get some samples tp proceed for a real test.
many thanks for your help.
Matt
2020-03-12 10:21 AM
Dear Matt,
it depends on your need. I will contact you directly to discus that.
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.