cancel
Showing results for 
Search instead for 
Did you mean: 

ST25RU3993-HPEV kit

RBhav.1
Associate

I am looking to use ST25RU3993-HPEV kit for my project. Does the STM32L476RGT6 MCU (Which is included in kit), has ability to program with C language ? IOT? does the Antenna has ability to communicate with Arduino/ESP32 ? I2C/SPI?UART?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Nick K
ST Employee

Hello RBhav.1,

To start developement based on the ST25RU3993-HPEV kit ST offers the schemantic of the board and the FW that is running on the board, both as open source. Please have a look at https://www.st.com/en/nfc/st25ru3993.html were all resources are available. 

Further details and resources on the STM32L476 that is used with the HPEV kit can be found at https://www.st.com/en/microcontrollers-microprocessors/stm32l4-series.html. ST also offers a set of software tools that allow to develop application for many use-cases including IOT applications written in C. 

It is also possible to use the ST25RU3993 together with other microcontrollers or system on chip solutions as ESP32. 

BR

View solution in original post

1 REPLY 1
Nick K
ST Employee

Hello RBhav.1,

To start developement based on the ST25RU3993-HPEV kit ST offers the schemantic of the board and the FW that is running on the board, both as open source. Please have a look at https://www.st.com/en/nfc/st25ru3993.html were all resources are available. 

Further details and resources on the STM32L476 that is used with the HPEV kit can be found at https://www.st.com/en/microcontrollers-microprocessors/stm32l4-series.html. ST also offers a set of software tools that allow to develop application for many use-cases including IOT applications written in C. 

It is also possible to use the ST25RU3993 together with other microcontrollers or system on chip solutions as ESP32. 

BR

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.