2023-05-29 12:49 AM
Editing ST25R3911B DISCO in STM32CubeIDE did not generate an error, but it cannot be read. How can ST25R3911B edit NFC in STM32Cube?
Solved! Go to Solution.
2023-05-29 1:23 AM
Hi:
The X-NUCLEO-NFC05A1 is an NFC card reader expansion board based on the ST25R3911B.
See X-NUCLEO-NFC05A1, UM2252, X-CUBE-NFC5 and UM2253
Rgds
BT
2023-06-07 6:26 AM
2023-05-29 1:02 AM
Hi
STSW-ST25R002 Firmware for ST25R3911B-DISCO kit (Source) is provided with a Keil µVision project file. The support of STM32Cube is not provided.
If you are looking for a development board with FW package available for STM32Cube, I would rather recommand to use the X-NUCLEO-NFC05A1 board and the X-CUBE-NFC5 FW package.
Rgds
BT
2023-05-29 1:15 AM
Can the X-NUCLEO-NFC05A1 board serve as a reader for reading data?
2023-05-29 1:23 AM
Hi:
The X-NUCLEO-NFC05A1 is an NFC card reader expansion board based on the ST25R3911B.
See X-NUCLEO-NFC05A1, UM2252, X-CUBE-NFC5 and UM2253
Rgds
BT
2023-06-05 7:24 PM
I am currently using X-NUCLEO-NFC05A1. Can I use X-CUBE-NFC7 to configure ST25?
2023-06-06 1:43 AM
Hi,
the FW package for the X-NUCLEO-NFC05A1 is X-CUBE-NFC5 not X-CUBE-NFC7.
Rgds
BT
2023-06-07 6:24 AM
Can STM32Cube add X-CUBE-NFC5? If possible, how can I add X-CUBE-NFC5?
2023-06-07 6:26 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.