2024-05-22 6:15 AM
Is it possible to adjust the slew rate of the RFO1/RFO2 outputs of the ST25R3916B?
Solved! Go to Solution.
2024-05-23 6:42 AM
Hi,
that is all information that I can offer. Just set d_tim_man=1 and cycle through the 5 d_tim values turn on the field and see if you observe a change.
BR, Ulysses
2024-05-23 4:57 AM
Hi,
what are you trying to achieve with changing the slew rate?
Driver behavior can be influenced by means of the bits in Tx Driver Timing Register (B 29h).
BR, Ulysses
2024-05-23 5:41 AM
I'd like to explore the possibility of reducing rise and fall time of the Tx outputs to reduce harmonics. (This would be in addition to correct EMC filter values, proper layout, optimization of AAT range per AN5322, etc.)
I see the Tx driver timing register described in section 4.5.51 of the datasheet, but there's not a lot of detail. Where can I find more information?
2024-05-23 6:42 AM
Hi,
that is all information that I can offer. Just set d_tim_man=1 and cycle through the 5 d_tim values turn on the field and see if you observe a change.
BR, Ulysses
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.