2020-01-17 2:57 AM
Hello,
I am evaluating the ST25R3916 solution for exclusive use in Card Emulation mode.
I need additional information on the part of passive components and matching circuits necessary to use only the Card Emulation mode.
As a reference I was seeing the X-NUCLEO-NFC06A1 board, do I need all the components on the X-NUCLEO-NFC06A1?
Any reference on this?
Best regards,
Damiano
Solved! Go to Solution.
2020-01-20 7:11 AM
Hi Damiano,
I had a chat with Carlo:
With the ST25 tags it is not possible to implement an arbitrary ISO7816-4 (non-NDEF) application. Even if you don't want to use reader functionality on the ST25R3916 you still need all the components. The only exception is the Variable Capacitors which you can remove / compensate with the MLCs.
Regards, Ulysses
2020-01-17 5:22 AM
Hello,
Also for card mode only it is required to use all passive components like in reader mode, including complete matching network.
If you only need card mode, maybe you can use ST25 dynamic tags instead?
Bye,
Carlo
2020-01-17 5:32 AM
Hello Carlo,
i need ST25R3916 for card emulation, there are others ST25 that offer this functionality?
Regards,
Damiano
2020-01-17 5:43 AM
Hello,
please have a look at this link:
Bye,Carlo
2020-01-17 5:48 AM
I have the problem wrote in this post: https://community.st.com/s/question/0D50X0000BsOJvASQW/application-non-ndef
There are ST25 dynamic tags that offer this functionality?
Thanks,
Damiano
2020-01-20 7:11 AM
Hi Damiano,
I had a chat with Carlo:
With the ST25 tags it is not possible to implement an arbitrary ISO7816-4 (non-NDEF) application. Even if you don't want to use reader functionality on the ST25R3916 you still need all the components. The only exception is the Variable Capacitors which you can remove / compensate with the MLCs.
Regards, Ulysses
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.