2020-04-07 4:44 AM
Dear ST Community,
I hope you are doing great.
I am having a trouble to run the GUI of ST25R3916 discovery board on my machine, I have windows 10 operating system, I tried to reinstall the included drivers (with the GUI), but the GUI is not able to recognize that the reader is connected to my PC. In the device manager when I connect the board I am getting the following drivers in my list:
Also I have used dfu-util to check if my system can identify the DFU, but It can not. I tried different PCs, but all have windows 10 OS. I am getting the same problem in all of them.
I would really appreciate your help.
Thank you very much.
Solved! Go to Solution.
2020-04-08 12:38 AM
Hi,
you need to connect the micro-USB plug and press the User button while powering. Only then it enters USB mode. This is also described in the user manual.
Regards, Ulysses
2020-04-08 12:38 AM
Hi,
you need to connect the micro-USB plug and press the User button while powering. Only then it enters USB mode. This is also described in the user manual.
Regards, Ulysses
2020-04-08 7:10 AM
Thank you very much,
this worked out.
I just wanted to mention that it is not clear in the user manual that the user button has to be pressed.
Many thanks again for your help.
2023-10-20 5:10 AM
Hi to all,
i have a similar problem: i want to connect the STEVAL-25R3916B to the discovery gui but, but this doesn't find /recognise the eval board.
I connect the mini-USB , and during the power on , i press the user button and the display shows me that the board is in USB mode. Then i launch the SW but it isn't connected to the eval..
In the device manager i find only a virtual com STlink, no more... is it enought?
i just already try to use micro-USB, mini-USB, then also togheter, changing the JA settings but without any good results
please help me
thanks
2024-05-02 7:02 AM
Hey,
Got the same error (ST-Link detected instead of STM device on DFU mode) and still can't get any solution on my 2 day researchs.
Is there someone who know how to resolve this issue ?
@logantenna do you have the solution now ?
Oh and I tried using the ST-link utility to make some test but I'm still not able to switch of device mode
And yes I am only connected with the USB port and the board's screen show the USB mode
Thanks,
Antoine, for Kuvee
2025-10-21 1:53 PM
Facing same issue.
2025-10-22 12:29 AM
Hi,
maybe emphasizing once more: You need to connected the micro-USB on the middle of the left side of the board. The mini-USB on the top left cannot be used for communication.
Regards, Ulysses
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.