2023-07-20 6:43 AM
I am currently using a mix of ST25R3916 and ST25R3916B with ST25RFAL002 v2.8.0.
In the default analog config table for the 3916 (rfalAnalogConfigTbl.h), under CHIP_INIT, there is an undocumented register that is being configured:
0x84U, 0x10, 0x10 /* Avoid chip internal overheat protection */
This does not appear in the default analog config table for the 3916B. It seems like disabling overheat protection is probably not what is intended since I don't see anything in the errata about any issues with overheat protection. That is just my assumption though, so I wanted to get some clarification on why this was being configured.
Solved! Go to Solution.
2023-07-21 12:45 AM
Hi,
the default ST25R3916-nonB analog configuration uses this internal overheat protection setting for normal operation. It should be kept if you have custom analog config.
Rgds
BT
2023-07-20 7:20 AM
Hi,
The setting 0x84U, 0x10, 0x10 is specific for the ST25R3916-nonB. See §2.4 in AN5584 ST25R39xx NFC reader thermal design for more information.
2023-07-20 8:37 AM
Ah, I see that now. AN5584 makes it seem like setting that register is just for measuring driver resistance. Does it need to be set for normal operation as well?
2023-07-21 12:45 AM
Hi,
the default ST25R3916-nonB analog configuration uses this internal overheat protection setting for normal operation. It should be kept if you have custom analog config.
Rgds
BT
2023-07-25 1:33 AM
Please see also DS12484 ch. 4.1: "To prevent the internal overheat protection to trigger below the junction temperature, the 3-byte frame FCh / 04h / 10h (register access / address / value) has to be sent after power-on and Set default command"
Regards, Ulysses
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.