2020-12-02 12:07 AM
I am looking for the source code of CR95HF.DLL.
The project successfully implements bidirectional comms between CH95HF hardware (which is based on the DEMO-CR95HF-A board) with a M24SR02-Y in the target device. We use CR95HF.DLL V1.2 with various Delphi-developed applications.
A problem has been observed when the applications are used in countries that do not use US English environments. The nul-terminated paraters used in the DLL calls appear to be an issue. Data appears to be modified IN the DLL with single characters appearing as two bytes (i.e. unicode representations)
My feeling is that modifying the DLL would solve this problem.
Solved! Go to Solution.
2020-12-02 5:21 AM
Hi,
thanks for using the CR95HF product. The source code of the CR95HF DLL will be provided to you in private.
Rgds
BT
2020-12-02 5:21 AM
Hi,
thanks for using the CR95HF product. The source code of the CR95HF DLL will be provided to you in private.
Rgds
BT
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.