2020-04-06 7:39 AM
Hello,
I am using ST25R3911 to read ISO15693 tags with the ST example from X-CUBE-NFC5. Everything works fine, now, I would like to read memory of Mifare Ultralight (without encryption). I know that st25 can't read Classic Mifare, but I don't find the code in the library to read blocks of Mifare Ultralight (ISO 14443). Does it exist ?
Thanks.
Solved! Go to Solution.
2020-04-07 3:12 AM
Hi,
you will need to add yourself the proper calls to rfalT2TPollerRead(). Out of the box it tries to read on a T2T the Capability Container according to NFC Forum T2T specification and based on its content tries to read the NDEF area.
Regards, Ulysses
2020-04-06 11:15 PM
Hi,
Mifare Ultralight follows NFC Forum T2T specification and can be formatted as a T2T (using e.g. the Manufacturers Android App). When formatted its content can be read using X-CUBE-NFC5 v2.0 (PollingTagDetectNDEF).
The low level access functions are implemented in rfal_t2t.c.
Regards, Ulysses
2020-04-07 2:37 AM
Hi,
Thanks for your quick answer.
Is it possible to read the tag out of box with X-CUBE-NFC5, but without formatted the tag as a T2T ?
Thanks.
2020-04-07 3:12 AM
Hi,
you will need to add yourself the proper calls to rfalT2TPollerRead(). Out of the box it tries to read on a T2T the Capability Container according to NFC Forum T2T specification and based on its content tries to read the NDEF area.
Regards, Ulysses
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.