cancel
Showing results for 
Search instead for 
Did you mean: 

Question about Send and Read of ST25R3916

DLuo.1
Associate II

Hello,

I am using the X-NUCLEO-NFC06A1 board to test the NFC functions, and to develop our prototyp NFC reader. I write the Firmware with other micro controller, and find it is really difficult to understand the ST25 Embeeded NFC library (STSW-ST25R16_v1.3.0). The codes are complicate and are not possible to use in my controller.

So read some other Q&A and try to use direct commands and set the registers and to realize the NFC read and write. The following is the current code. ST25R3916 can read and transmit some bytes, because the main interrupt register shows start of receive, end of receive and end of transmission. But it can only receive 2 Bytes like 0x0008.  

My question is How can I read the UID and complete data of tag? and how to write data to the tag correctly. Can anyone give a help? Thank you very much.

ST25R3916_Init(void)

{

 ST25R3916_Set_CMD(0xC1);//Set default

 ST25R3916_Set_CMD(0xDF);//Measure power supply

 ST25R3916_Set_Register(0x00,0x07);//Differential, SPI and MCU_CLK disabled

 ST25R3916_Set_Register(0x01,0x1C);

 ST25R3916_Set_Register(0x02,0xCF);//enable oscillator

 /*Wait until the interrupt shows that the oscillator is stable (IRQ when oscillator frequency is stable)*/

 ST25R3916_Set_Register(0x03,0x08);

 ST25R3916_Set_Register(0x08,0x50);

 //ST25R3916_Set_Register(0x0A,0x10);

 ST25R3916_Set_Register(0x0B, 0x08);

 ST25R3916_Set_Register(0x0F, 0x0E);

 ST25R3916_Set_Register(0x11, 0x23);

 ST25R3916_Set_Register(0x12, 0x20);

 ST25R3916_Set_Register(0x13, 0x02);

 ST25R3916_Set_Register(0x14, 0xC8);

 ST25R3916_Set_Register(0x15, 0x80);

 ST25R3916_Set_Register(0x16, 0x83);

 ST25R3916_Set_Register(0x17, 0xBF);

 ST25R3916_Set_Register(0x18, 0x0F);

 ST25R3916_Set_Register(0x19, 0xFB);

 ST25R3916_Set_Register(0x23, 0x30);

 ST25R3916_Set_Register(0x25, 0xDD);

 ST25R3916_Set_Register(0x26, 0x82);

 ST25R3916_Set_Register(0x27, 0x82);

 ST25R3916_Set_Register(0x28, 0x70);

 ST25R3916_Set_Register(0x29, 0x5F);

 ST25R3916_Set_Register(0x2A, 0x11);

 ST25R3916_Set_Register(0x31, 0x10);

 ST25R3916_Set_Register(0x2A, 0x11);

}

while(1)

{

ST25R3916_FIFO_Write(); // write data to the fifo to send

Write_CMD(0xC2);// Stop all activities

Write_CMD(0xD5);//Reset RX gain

Write_CMD(0xC6);//Transmit REQA

delay_ms(500);

}

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

Hi,

If I am not wrong, TI CC2540 has 2 SPI so I would recommend to use SPI communication rather than I2C. Anyway, the platform.h has also wrapper macros for I2C configuration. Make sure to use RFAL_USE_I2C macro definition when compiling the ST25R3916 driver for I2C. On HW side, make sure to have the I2C_EN pin being properly configured for proper interface selection.

The flash size and RAM size needed for the RFAL depends on enabled features (e.g. do you need all NFC technologies or only NFC-A?). The selection of the various features is achieved through the platform .h file. Code for disabled features is removed at compile time and this reduce the RAM/Flash resources accordingly. The rfal.chm documentation file contains the size of each compiled module (based on STM32 MCU). This can give a first estimate of RAM/FLASH needed.

The rfal.chm documentation file also contain information about the configuration and the porting of the RFAL

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Brian TIDAL
ST Employee

Hi,

which MCU do you use?

The RFAL Firmware from the ST25 Embedded NFC lib is designed to be portable across different MCU. Wrapper macros are provided in platform.h so that you can adapt the SPI/GPIO/etc. management to your own MCU. If you already have a functional SPI communication between the MCU and the ST25R3916, porting the RFAL on your own MCU should be quite straightforward .

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Thanks a lot for the reply,
I am using the TI CC2540, 8051 MCU, and I2C Bus. is the TI CC2540 is small for the NFC Lib?
In the NFC Lib, which head file or C file is for adapt of I2C Bus?
Best Regards
Dongfeng Luo
Brian TIDAL
ST Employee

Hi,

If I am not wrong, TI CC2540 has 2 SPI so I would recommend to use SPI communication rather than I2C. Anyway, the platform.h has also wrapper macros for I2C configuration. Make sure to use RFAL_USE_I2C macro definition when compiling the ST25R3916 driver for I2C. On HW side, make sure to have the I2C_EN pin being properly configured for proper interface selection.

The flash size and RAM size needed for the RFAL depends on enabled features (e.g. do you need all NFC technologies or only NFC-A?). The selection of the various features is achieved through the platform .h file. Code for disabled features is removed at compile time and this reduce the RAM/Flash resources accordingly. The rfal.chm documentation file contains the size of each compiled module (based on STM32 MCU). This can give a first estimate of RAM/FLASH needed.

The rfal.chm documentation file also contain information about the configuration and the porting of the RFAL

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Thank you very much for your Information and help. I will try later.
Best Regards,
Dongfeng
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.