2025-10-30 9:02 AM
Hi,
is there a polling-only Linux C code example for the X-NUCLEO-NFC09A1? The demo app is IRQ based and we plan to use many readers so it would be convenient to save the IRQ pin and use only the CS pin per device.
Regards.
Solved! Go to Solution.
2025-11-03 2:30 AM
Hello myso,
nothing available out of the box. You can try and change st25r200WaitForInterruptsTimed(): Set the experimental ST25R_POLL_IRQ and see if this is already sufficient (was in the past).
BR, Ulysses
2025-11-03 2:30 AM
Hello myso,
nothing available out of the box. You can try and change st25r200WaitForInterruptsTimed(): Set the experimental ST25R_POLL_IRQ and see if this is already sufficient (was in the past).
BR, Ulysses
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.