2023-10-09 7:31 AM
I'm using a DLP-RID2 device to write and read data in a ISO 15693 TAG, in particular i'm using tags based on the ST25TV02KC which have 320 bytes of information arranged in 80 blocks of 4 bytes each.
My problem is that with a new factory TAG, i can't read block 50, and read/write operations don't works.
Do you have any suggestions for any commands to use to be able to use all 80 blocks?
I attach a log that illustrates the commands sent for a read
Best regards
Solved! Go to Solution.
2023-10-09 8:11 AM
Hi,
I think you need to increase the address to be read in hexadecimal like this: 00 01 02 03 04 05 06 07 08 09 0a
Your last successful reading is from address 0x49=73 and then with 0x50 you are jumping to 80 which doesn't exist anymore.
Best Regards, Ulysses
2023-10-09 8:11 AM
Hi,
I think you need to increase the address to be read in hexadecimal like this: 00 01 02 03 04 05 06 07 08 09 0a
Your last successful reading is from address 0x49=73 and then with 0x50 you are jumping to 80 which doesn't exist anymore.
Best Regards, Ulysses
2023-10-10 12:15 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.