2017-11-15 8:34 AM
Hi,
we are trying to using the ST25DV64K to implement the reading and writing data via RF between the ST25DV64K and Android device.
The area 3 is protected by RF password 3 with default password .
Tried to use the below code to open the RF security session but always return �(byte)0x01�. Could you advise ?
It would be appreciated if the sample code of reading and writing the data on the protected Area is also provided.
Thanks.
public static byte
[]SendPresentPasswordCommand
(Tag myTag, byte
PasswordNumber, byte
[] PasswordData,
DataDevice ma){byte
[] response =new byte
[] {(byte
)0xFF
};
byte
[] PresentPasswordFrame;
PresentPasswordFrame =
new byte
[]{(byte
)0x02
,
(byte
)0xB3
,
(byte
)0x02
,
PasswordNumber,
PasswordData[0
],
PasswordData[1
],
PasswordData[2
],
PasswordData[3
]};
PresentPasswordFrame =
new byte
[]{(byte
)0x02
,
(byte
)0xB3
,
(byte
)0x02
,
(byte
)0x03
,
(byte
)0x00
,
(byte
)0x00
,
(byte
)0x00
,
(byte
)0x00
};
int
errorOccured =1
;
while
(errorOccured !=0
) {try
{ NfcV nfcvTag = NfcV.
get
(myTag);
nfcvTag.close()
;
nfcvTag.connect()
;
response = nfcvTag.transceive(PresentPasswordFrame)
;
if
(response[0
] == (byte
)0x00
|| response[0
] == (byte
)0x01
)//response 01 = error sent back by tag (new Android 4.2.2) or BC
{ errorOccured =
0
;
//Used for DEBUG :
} }
catch
(Exception e) { errorOccured++;
//Used for DEBUG :
if
(errorOccured ==2
) {//Used for DEBUG :
//Used for DEBUG :
return
response;
} } }
return
response;
}#st25dv64k #androidSolved! Go to Solution.
2017-11-21 5:23 AM
Hi Don,
On ST25DV64K the Area password is 64 bits long. Here is the command that you can use:
02 b3 02 03 00 00 00 00 00 00 00 00
Best regards
Olivier
2017-11-21 5:23 AM
Hi Don,
On ST25DV64K the Area password is 64 bits long. Here is the command that you can use:
02 b3 02 03 00 00 00 00 00 00 00 00
Best regards
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.