2020-04-02 2:28 PM
I would prefer range over data rate and was wondering if the NFC forum matching from the ST25R3911-DISCO board would apply to the 3916?
Solved! Go to Solution.
2020-04-03 2:00 AM
Hello SSita,
This is not possible. Both matchings are designed for different antennas. Therefore they cannot easily exchanged. To increase the output power / read range, please follow AN5276 - Antenna design for ST25R3916. The Q-factor should be choosen as high as possible according to the supported bit rates and the target matching impedance can be lowered. AN5276 should give some guidance about the selection.
BR Travis
2020-04-03 2:00 AM
Hello SSita,
This is not possible. Both matchings are designed for different antennas. Therefore they cannot easily exchanged. To increase the output power / read range, please follow AN5276 - Antenna design for ST25R3916. The Q-factor should be choosen as high as possible according to the supported bit rates and the target matching impedance can be lowered. AN5276 should give some guidance about the selection.
BR Travis
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.